LTE FDD

CFI (Downlink E-UTRA)

For Waveform Playback (ARB) capability.

This topic describes the settings of the CFI node when the carrier is Downlink E-UTRA.

State

Power

Scrambling

CFI

State

Turns the CFI channel state On or Off.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CFI:STATe ON|OFF|0|1

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CFI:STATe?

SCPI Example

RADio:LTEFdd:WAVeform:CCARrier:DLINk:CFI:STATe ON

RADio:LTEFdd:WAVeform:CCARrier:DLINk:CFI:STATe?

Choices

ON | OFF

Preset

1

State Saved

Yes

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

Power

Sets the power level for the CFI channel.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CFI:POWer <rel_ampl>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CFI:POWer?

SCPI Example

RADio:LTEFdd:WAVeform:CCARrier:DLINk:CFI:POWer 0

RADio:LTEFdd:WAVeform:CCARrier:DLINk:CFI:POWer?

Notes

Power level, in dB relative to the reference signal power.

Preset

0

State Saved

Yes

Min

-60

Max

20

Initial S/W Revision

A.20.01

Scrambling

Turns scrambling On or Off for the CFI channel.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CFI:SCRambling ON|OFF|0|1

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CFI:SCRambling?

SCPI Example

RADio:LTEFdd:WAVeform:CCARrier:DLINk:CFI:SCRambling ON

RADio:LTEFdd:WAVeform:CCARrier:DLINk:CFI:SCRambling?

Choices

ON | OFF

Preset

1

State Saved

Yes

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

CFI

Query only

Displays the Control Format Indicator value for each slot.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<channel>:DLINk:CFI:VALues?

SCPI Example

RADio:LTEFdd:WAVeform:CCARrier:DLINk:CFI:VALues?

Notes

Values correspond to the number of OFDM symbols used for PDCCH transmission in a subframe. Set via PDCCH Allocations.

Preset

"3,3,3,3,3,3,3,3,3,3"

State Saved

No

Min

N/A

Max

N/A

Initial S/W Revision

A.20.01

Carrier Downlink ARB

Welcome to LTE FDD